This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM63615-Q1: VIN to GND Negative pressure slightly exceeds the standard to assess the risk

Part Number: LM63615-Q1

Tool/software:

Hi  team,

When the customer powers on, the VIN negative pressure will slightly exceed the standard. Please help evaluate whether there is a risk in the risk assessment.

See below test result :

From 0 to -0.3V , 5.8s;

From -0.3V to -0.38V 2.7s.