Part Number: UCC28704
Tool/software:
Hi there,
we are designing a new product which requires a 230VAC to 5V DC with 2.5A of current rating, and we found that the flback controller part "UCC28704DBVR-1" is best suit for us,
In that we have few doubts please answer the same.
1, We found there is a difference in EVM baord ("UCC28704EVM-724 10-W USB
Adapter") schematics and a TI work bench schematics, the Zenner Diode DZ in Work bench is not available in EVM baord. pelase confirm which schematics should we follow

2, The Maximum recommended voltage applied across the VDD = 38V as per the datasheet. But in both the schematics the VDD Pin is directly exposed to the 200V DC, Could you please confirm that do we need any other additional measures to overcome this issue ?

3, How to finalyse the trickle resistor value in the SLU603B Calculation sheet only the user input colum is there but there is no actual calculated value is available.

Thanks in advance for your response,
Sakthivel