Tool/software:
Question 1: about ILIMIT calculation
Per data sheet:
![]()
I am having some difficulty to correlate the result of equation above with RLIMIT=80.6k (ILIMIT=9.24A) with graphs on Figures 18 and 19 and values on the specifications (section 7.5):

Could you provide some explanation for the apparent (to me) discrepancies between the formula, graphs and table? What am I missing?
Question 2: what value should I use?
According to my understanding of the diagrams of the data sheet, the limit should be set based on the peak inductor current. Per my math and Webench, maximum peak inductor current (min Vi, max output current) is ~4A during startup. Based on this and giving 50% tolerance to deal with component variation (guestimate based on the table excerpt above), I would set the current limit to 6A. However, Webench sets the RLIMIT to 86.6k, ~8.7A per the formula above, 8.9A per Webench panel, way above the 6A I would use.
What am I missing?
Thanks in advance.