Other Parts Discussed in Thread: BQ25606
Tool/software:
Hi TI,
I am having below requirements for my portable wifi extender project.
1. The system is powered by a 3.7V Lipo 1800mAh battery, that should be chargeable using a USB input.
2. The voltage of battery and USB should be cut down to 3.3V and should be given to my system (it doesn't draw more than 700mA)
3.I don't want to use I2C to control the BQ25895. I simply want to configure it to charge my battery by default and seamlessly switch the output from battery to USB using the power path feature. Can the IC be configured to do that without any software configuration I want a plug and play solution?
4. Would you recommend configuring the IC to generate 3.3V when both USB and battery are present to power my entire load? Or should I boost the 3.7V from the battery to 5V and use an external LDO to further reduce this boosted 5V to 3.3V? I want to know if your IC can directly regulate the USB/3.7V battery voltage (even when the battery voltage drops to around 3.4V).
5. I want to know if my load should be connected to the PMID pin? or SYS pin, i believe it's PMID but want to still cross-check
6. If software configuration is mandatory for my IC, then can you recommend me some other part number that is more of a plug and play solution?