Part Number: LM74930-Q1
Tool/software:
Hello TI team,
As the title question,
-
70 load-dump testThe parameters are as level2 ,The peak of pulse is Up70V.Supply Voltage is 58V.The pulse will keep td 0.5ms with Ri 0.2ohm input resistance.

The max working DC votage level is 58V. Is it possible to use LM74930-Q1 to clamp down down the load-dump pulse below 60V. Or some other chips could be suggested?
Thank you!