Other Parts Discussed in Thread: LMG1205, LM25149,
Tool/software:
I want to simulate a design with LM25149-Q1 using PSpice for TI. I start of using the project provided with the spice model of LM25149-Q1. For my simulation I want to follow the LM25149 controller with a GaN FET driver LMG1205. For this I do not need the bootstrap circuitry of the controller. Ho should be around 4-5V when pulled high. I've been able to do this by grounding SW pin. When I do this however the LO output of the controller becomes very strange. It is a pulsed signal with very thin pulses. See images attached. Of course I changed the high side mosfet for a voltage controlled switch, the HO can't drive the mosfet without bootstrap. My idea is to ultimately have the GaN driver here in between. But the pulses get messed up when grounding SW. Any assistance is highly appreciated.
Kind regards,
Rauf