This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5023: LM5023 light load issue

Part Number: LM5023

Tool/software:

Hi team,

customer tesed LM5023 and got some issue here.

Red is VGS

Grees is VDS.

Is this waveform normal?This waveform is different from what I know.

Condition 100VAC  Vo=15V 0.1A or less

  • Hello,

     

    Your inquiry has been received and it will be addressed in the order that it was received.

     

    Regards,

  • Hello,

    Your design seems to be going from 50% duty cycle to a minimum duty cycle. I am not sure what is causing this bursting.  It could be noise on the QR causing the FET to turnoff or and instability.

     

    Could you probe Comp, CS, VCC Out during this condition with an oscilloscope?   It is important to have them all on the same plot.

     

    If you want to share a schematic, I will review it for you as well?

     

    Regards,

  • Hi team,

    100VAC

    264VAC

  • Hello,

     

    I think you might have noise on the QR pin make the controller think zero current is reached and turning off the gate drive.

     

    In your evaluation you might want to swap VCC for the QR pin to verify?

     

    If it is noise on the QR pin then you should be able to resolve it by adding some capacitance to the QR pin.  You might even see that just probing the QR pin removes the issue.  If it does than 10 pF of capacitance would fix the issue.  This is because the scope probe capacitance is generally around 10 pF.

     

    Regards,

  • hi Sir

    add the 220p cap between the QR Pin, still cut off

  • Hello,

     

    You might want to study QR, Comp, CS and VDD with an oscilloscope to see what they look like to verify there is no noise on the QR pin.  I would study before and after adding any capacitance.

     

    If the noise is not present from the waveforms than the next place to look at is loop stability.  You will need to check it with a network analyzer to make sure you enough phase margin at cross over (> 45 deg) and enough gain margin less than – 3 dB.

     

    Regards,