This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: LED burned issue

Part Number: TPS61165

Tool/software:

Hi Team, 

1. What is the maximum receive current specification for this driver IC?
2. According to datasheet the current limit is 1.2A. When exceeding this current, will the LED driver shut down? If not, when input 280mA, will the LED driver supply the LED directly?
3. On the other hand, if the LED driver does not supply large currents directly, but lowers the current to the LED, that inrush current may be in the LED driver to LED section
May I know if the LED driver IC supplies the LED this segment has a fuse? Are there specifications?