Other Parts Discussed in Thread: AWR1843AOP
Tool/software:
HI, TI
I am using the LP87524J-Q1 and have a few questions.
1.Currently, I am supplying 5V to BIN_BX and VANA of the LP87524J-Q1. In the datasheet, the maximum voltage for SCL and SDA is listed as "VANA with 3.6 maximum." Does this mean that VANA can handle up to 3.6V, and SDA/SCL pin should not exceed 3.6V ? I am having trouble understanding this, so please explain.
2.When using VVANA = VVIN_BX = 5V and the PMIC output is 3.3V,
how can I determine the minimum value? The datasheet is based on VVANA = VVIN_BX = 3.7V, so I have this question.
I look forward to your response. Thank you.