Does anyone know the minimum overhead voltage required for 5 VDC output for the LMZ22003?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does anyone know the minimum overhead voltage required for 5 VDC output for the LMZ22003?
Thanks
When the part is running off the internal clock at 800Khz the following chart from the datasheet can be used to determine minimum input voltage. The number in this table is very conservative and based upon the 5 amp version of the part, tested over temperature.
When the part is synchronized to an external clock. Use the following equation as a first pass.
Minimum Vin = Vout / (1 - 500e-9 * switching frequency).
Example
For 5V out and a switching frequency of 650Khz.
The minimum Vin would be around
5V / (1 - 500e-9 * 650KHz) = 7.4V