Tool/software:
Dear TI,
I would like to request a review of the following design. The goals of the design are as follows:
- Dimming of 12x Cree XP-G4 High Intensity LEDs in series
- 42V input
- Hybrid dimming (ADIM/HD pulled to ground)
- 1kHz PWM signal
- 1.5A max current
- Smooth low end dimming with no flickering
I have closely followed the second application example provided in the datasheet as it seems to fit my needs. All values have been calculated from equations provided.
Questions:
- What switching frequency should be chosen to achieve this (currently I am using 1MHz, which gives a 10uH inductor, is this wise?)
- Are there any guidelines for choosing an appropriate diode.
- Are my UVP resistors suitable
- Is any additional input capacitance required?
- Cflt is 2.2uF on the evaluation board, and 1nF on the datasheet. This is a very large discrepancy. Why?
- Ccomp is 10nF on the evaluation board, but 1nF on the datasheet. What is the reason for this discrepancy?
- With 0603 components, the passive capacitors aren't that close to the IC (see the first picture), is this an issue?
Notes:
- All passive components are 0603, except for the 1uF output capacitor (0805) and the input electrolytic capacitor.
- Fault is pulled to ground.
- ADIM/HD is pulled to ground to enable hybrid dimming.