Other Parts Discussed in Thread: UCC21710
Tool/software:
Hi there,
we designed a 3-phased inverter using a SiC MOSFET and six UCC21750 drivers. We use a half-bridge driver with two UCC21750 per PCB. The simplified design is shown below.
The inverter works well up to ~750V DC. Above 750V DC we see that the bottom FET is no longer turned on reliably. For the first example, we measured:
CH1: current (no load)
CH2: IN-
CH3: Gate
CH4: IN+
The example shows the Gate being turned on in the beginning and then in the second clockcycle the Gate is initially turned on, then falls off, rises again and then stays low.
There is quite some noise on the signals. We don't have a opto coupled isolated probes so it might be a measurement problem... Here is a comparison of a working turn on and a non working:
Since the noise on the working turn on is quite similar to the non-working one (and the difference of In+ - In- is not affected by the oscillation) we suspected the DESAT (although we did not get a Fault from the driver).
I switched to non isolated probes measuring only the high voltage side:
CH1: current
CH2: VDD
CH3: Gate
CH4: DESAT
With a valid turn on we get ~5.5V at the DESAT pin which is well below the 9.15V threshold. The big oscillations are gone with the non-isolated probes and the signals seem to be fine. Still we will also get non working turn ons, even with no probes connected.
We went on measuring the RDY pin, changing to isolated probes again:
CH1: RDY
CH2: IN+
CH3: Gate
CH4: IN-
Since it does not go or stay low, we measured the Fault and Enable pins:
CH1: Gate
CH2: IN (IN+ - IN-)
CH3: Fault (Pin 13)
CH4: EN (Pin 14)
The Fault Pin drops a bit during the turn on, but the Gate rises. After ~6µs the gate turns off but IN, EN and Fault are completely stable at this point.
We also found out, that the driver is working with some duty cylces and will continue to not work for ~550µs once it stopped working before trying to turn on the gate again.
CH1: Gate
CH2: IN
I marked in green the areas of the duty cycle where the driver was working, and in red the ones where it didn't turn on the gate. Especially interesting are the short pulses after 550µs staying low where it tires to turn on the gate but shuts it down again before the IN signal falls low.
I'm quite out of Ideas what to measure on the driver PCB. We will now try to reduce the coupling capacitance of the AC-High voltage to the Low-Voltage side by adding CMCs in the supply and separating the high and low side driver, since we only get this behavior on the low side. I would highly appreciate it if you could give us a hint on how we could get rid of this problem.
Kind regards
Bernhard Baier