This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431-Q1: TL431-Q1

Part Number: TL431-Q1

Tool/software:

Hello Team,

I am looking for the voltage reference IC. Which is having below specification:

Vin= 12V to 24V 

Vout = 0.5V to 0.8V

tolerance= 0.1% to 1%

Qualification= Automotive qualified AEC-Q1

current capability 25mA  

Best Regards,

Suma