Part Number: TPSI3050-Q1
Other Parts Discussed in Thread: TPSI3050
Tool/software:
Hello Team,
We are using the IC TPSI3050-Q1 in one of our products.
The attached is the schematic of the same.
The device is working in 2 wire mode,

The GPIO_275 is from a 3.3V GPIO pin of a controller and when we assert the pin, we are getting a 12V at the EN pin of the TPSI3050-Q1.
But still we are not getting +10V across TP11 and TP9. But instead we are getting +3V only.
But sometimes we will get +10V across these test points and the FET will turn ON.
1). What could be the reason for this?.
2). Is there any reason if we give 12V at the EN pin is the device is working in 3 wire mode?.
We have not given any voltage source or load at either end of the MOSFET. We are just checking the electrical resistance between the DRAIN of the MOSFET.
Looking for your reply.