Tool/software:
Hello
The datasheet of the TPS55287-Q1 states that the output can be adjusted up to 22V.
On the other hand, when setting REF to max (1200mV) and INTFB ot min (0.0564), the output voltage is about 21.2V according to Vout=Vref/INTFB.
What can be done to reach the 22V as stated in the datasheet?
Is it done by using external voltage feedback? Or by changing the CDC (cable voltage droop compensation)?
Are there other (new) alternative parts, which would allow a higher programmable output voltage (I mean in-application programmable, to change the output on the fly)? Needed current is below 1A, nominal Vin is 24VDC.
Best Regards
Gerardo