This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: Equivalent device with lower insertion time

Part Number: LM5069
Other Parts Discussed in Thread: TPS1685

Tool/software:

Hi,

We are using in one of our design the LM5069.

However, the device has a single pin allowing to set both inrush and insertion time which is an issue for us as we can't tweak both parameters independently and thus leading to an important insertion time at power-up.

Is there an equivalent device with the capability to set the two parameters separately ?

We also need it to be capable of sustaining polarity inversion on the power input.

Context here: e2e.ti.com/.../5726013

Clément