Other Parts Discussed in Thread: TPS1686, TPS25984B
Tool/software:
In our application we need to fuse the load at 0.9A.
However, the load is allowed to use 5.5A for 20ms. During the 20ms at 5.5A the fuse should not trip.
How can we make the TPS2663x act more like a slow blow fuse?
Not sure, but it seems the I_lim pin output a current, relative to the output current.
Is it allowed to place a capacitor over R_limit, so decrease the voltage rise over R_limit, during the current peak?
Regards, Hans