Tool/software:
Hello,
I am planning to use the TPS26630 in parallel as my load current is more than 6A. I would like my system to be protected from reverse polarity but i also want to control the load ON/OFF using the SHDN pin.
Added to the load i have another uC that i don't it to be shutdown as it will control the efuse. If i connect the DC/DC and the uC from the IN pin of the fuse will my system (DCDC + uC + Load) still be protected from reverse polarity? If the SHDN is enabled and the load is switched off will that also cause the FET Q1 to switch off too and my uC will be switched off too?
Thank you very much for your support.