Part Number: LM61495-Q1
Tool/software:
Hi,
I am using LM61495-Q1 for our application.
Vin = 24V, Vout = 5V, Iout = 8A.
I need to margin the output voltage via external DAC. May be +10% to -10%.
Could you please tell me, how can I connect the DAC output in order to change the Vout of the LM61495-Q1? 
I am attaching the circuit which I used
And also, please suggest a voltage DAC for margining it
Thanks