This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: How to build an UPS with BQ25730 and constant output voltage, independent of cell count.

Part Number: BQ25730
Other Parts Discussed in Thread: , DAC53701

Tool/software:

Dear TI team.

I have a basic and general question about your battery charger solutions, specially the BQ25730.

We are currently working on a design which should work as a 12V (alternatively 24V) uninterruptible power source.

Under normal conditions, an adapter is delivering 12V (24V) to power the system and is connected to the input side of the BQ25730.

In my understanding, we have to connect the load to the input side of the BQ25730 as well.

I guess that, because on the output side of the BQ25730 we will probably not see 12V (24V), the voltage here depends on the charging voltage / cell count / cell charge state.

Am I right so far?

Additionally, if the adapter does not deliver power anymore, we will only see the battery voltage on the output side of the BQ25730, which is probably NOT 12V (24V) as well (depending on cell count and cell charge).

If the BQ25730 now switches to reverse mode, it will deliver 12V (24V) on the input side of the chip, right?

This can be done in USB-OTG mode, but switching fromnormal to reverse mode USB-OTG takes probably too long to deliver uninterrupted power (200ms or so I saw in the data sheet).

Only FRS would be faster (150us), but I understand FRS can only deliver 5V on the input side of BQ25730.

So, I'm a little lost and wondering if a UPS which always and under any circumstances delivers 12V (24V) can be build with a BQ25730 only and I would appreciate support here a lot.

If FRS could deliver 12V (24V) on the input side, everything would be fine.

Otherwise I only see the chance to add an additional DC/DC converter (buck/boost; maybe TPS551892 or so) on the output side of BQ25730 to convert voltage from battery and/or adapter to 12V (24V).

Again, the goal is to always deliver 12V (24V) (because system relies on those voltages), no matter if we get power from adapter of battery.

I hope I explained things good enough to follow and looking forward to your help.

Best regards,

Alexander W. Lenhardt