This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060: tps63060

Part Number: TPS63060

Tool/software:

HI,

Title: Issue with TPS63060 Buck-Boost Converter – Output Voltage Fluctuation

Description:
I am using the TPS63060 buck-boost converter with the following configuration:

  • EN (Enable) pin is directly connected to VIN
  • PG (Power Good) pin is connected to GND
  • PS/SYNC pin is connected to VIN
  • Feedback resistor values: R1 = 1MΩ, R2 = 110kΩ

Despite this setup, I am not getting a stable 5V output. The output voltage is fluctuating


Regards
Syam