Tool/software:
Hi,
I am using the TPS63060 buck-boost converter with the following configuration:
- EN (Enable) pin is directly connected to VIN
- PG (Power Good) pin is connected to GND
- PS/SYNC pin is connected to VIN
- Feedback resistor values: R1 = 1MΩ, R2 = 110kΩ
The issue I am facing:
- The output voltage is fluctuating instead of providing a stable 5V.
- When the input voltage exceeds 5V, the IC shuts down.