Tool/software:
Hi
I am using TPS25940-Q1 as e-Fuse for short circuit protection. I want to minimize the component counts due to space constraints, so I have connected PGTH, DEVSLP & OVP to GND, and left IMON, FLT, PGOOD floated. Will there be any issue connecting the mentioned pins to GND, as in datasheet nothing is mentioned for PGTH if not used?
I have attached the snap of circuit for the reference.
Also, I want to cut-off the output completely in case of any circuitry, auto-retry is OK, but it should only cutout the output. Datasheet says it limit the output in case of overcurrent and cutout the output in case of short circuit, but only for few microseconds. But in fig. 10.14 it can be seen that it it completely cutout the output till the current is limited.
So does it means it will keep the output cut if the I_load is greater than I_fastrip?
Thanks
Ritik