Tool/software:
Hello,
We are intending to use the LM5158 to generate a 45V regulated power supply from our 20V to 32V input power supply.
The 45V is used to generate further secondary supplies and to cope with the potential input power loss we have a big 680uF capacitor (750uF total on the on the power supply output.
The boost converter will be enabled after the input power supply reaches steady state.
So the first inrush induced by the capacitor is managed by the soft start from an eFuse we have before the boost converter.
The second inrush, when we start the boost converter will be managed by the LM5158 soft start.
The excel file that you provide is a bit misleading for computations, indeed it's not possible to select a mode where the part is started afterwards.
As-is, the file would suggest me to implement a 1,125µF capacitor but I believe it's because it considers my voltage is raising from 0V to 45V, right ?
While it should consider the raise from 20V (worst case) to 45V.
Am I assuming correctly ?
Thus the capacitor would rather be somewhere in the 680nF range.
Best regards,
Clément