Other Parts Discussed in Thread: LM74912
Tool/software:
Hello,
I am designing a board with two LM74912 controllers in an O-Ring configuration to power a single board from two batteries.
The system is intended to remain in sleep mode by default and wake up upon an external event.
In sleep mode, the always-on output will need to provide less than 100mA.
Does the LM74912 provide reverse current protection when both of them are used in an O-Ring configuration in sleep mode?
Thank you.