Other Parts Discussed in Thread: BQ25628E
Tool/software:
Hello,
I have been trying to implement the TPS2662 e-fuse IC on a board and am encountering some issues. For context, the circuit that this e-fuse is a part of is intended to be a charge base for a portable device. It takes a DC power source and passes it through to the portable device's charge contacts. Below is the circuit I have implemented:
OVP Target: 16.56V
UVLO Target: 5.95V
I limit: 760mA

This circuit is supposed to take in 8V to 15V and pass it though to the output charge contacts. The issue I am encountering is that this circuit is struggling at its maximum output voltage of 15V. The output either perpetually drops in and out or just clamps to ~2.5V.
Generally, if I provide the circuit with 12V input power things behave as expected.
Sometimes this circuit also behaves as expected when there is no load on it. I see the 15V at the output, but once I connect the circuit that is to be charged the efuse activates.
Downstream of this circuit we are using TI's BQ25628E with TI's recommended configuration from its datasheet in the portable device that is being charged. This is in a separate circuit board that is plugged in and removed from the circuit the e-fuse is in.
Another thing I have noted, which I do not want to rely on this in practice is if I touch the set resistors (R5, R6, and R7 in schematic) then I can activate and deactivate the protecting functions. This is not a desirable behavior.
Given all that information, here are the questions I am seeking assistance in answering:
- How can I get this efuse to consistently output 15V without dropping out?
- How do I prevent contact with the set resistors from affecting the efuse behavior?
- Is this device appropriate for a hot-swap charger base application?
Thank You,
Wesley Mandel