Other Parts Discussed in Thread: UCC28180
Tool/software:
Hi,
So my architecture is something like this:
Mains -> filter + inrush limiting -> rectifier-> UCC28180DR APFC --> UCC256601 LLC
I plunged in the design and i saw what I expected after the rectifier BUT when i did check the high voltage capacitors after the APFC stage they were well under the 390-400Vdc i was expecting so the UCC28180DR was not working properly for sure.
I did check that the Chip is powered, there were about 13V on the Vcc pin ( from a small aux power supply that i built in just in case) but still no sign that the UCC28180DR was doing anything.
The FB pin was at about 4-4.1V far lower then the 5V FB reference so i was sure my FB resistor math was still ok.
BTW there was no load connected to the SMPS the only power draw was the board itself . Nothing seemed to get hot ( except the NTC but that is supposed to get a bit hot at start up).
Any advice on what i should check? Should i post a schematic out here? ( i mostly did copy from a reference design + used the excel calculator provided by TI to validate my component choices)
Best regards