This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25019: LM25019SD/NOPB

Part Number: LM25019
Other Parts Discussed in Thread: LM25017

Tool/software:

Hello, everyone.
My project uses LM25019SD/NOPB. The schematic diagram is as follows. In the case that there is no load power consumption at the back end after power-on (FB1, FB3, and FB5 are removed), the chip input voltage is 24V and the working current is 19mA. If the current is too large, is there any way to adjust the chip power consumption and reduce the circuit? 

Thanks,

Ivy