This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR60440-Q1: Spread spectrum

Part Number: LMR60440-Q1


Tool/software:

In my circuit, FPWM mode is selected by default (mode pin connected directly to RT), when probed at the sw node, i could see duty cycle only varying at fixed switching frequency, when no load is connected. I have attached the oscilloscope image. I used the cursor to check the frequency of the given image, everywhere it was the same, only duty cycle was varied.
 
But in the datasheet it is mentioned as , when FPWM mode is selected at no load conditions, spread spectrum is active and should be visible. My set frequency is 2.2MHz and accordingly i should see the spread spectrum from 2.2MHz to 2.552MHz (16% from the set frequency - from datasheet - is it correct?)

Could you please let me know on the above issue?