Part Number: LM4041-N
Tool/software:
Hi team,
We want your opinion about below added explanation in new revision detasheet of LM4140-N.
"When the output voltage, VZ, is set below 2.5V on adjustable versions of LM4041-N and LM4041-N Q1, the device can experience increased reference voltage change with output voltage change (ΔVREF/ΔVKA) when compared to output voltages set equal to or above 2.5V"
Q1. In this explanation, Vz is same meen with Vka?
Q2. In LM4041-N datasheet, the characteristic of ΔVREF/ΔVKA is wote as ΔVREF/ΔVZ. Is this understanding correct?
In other datasheet(LM4041), ΔVREF/ΔVKA is defined by Iz. However, in LM4041-N, ΔVREF/ΔVZ is defined by IR like below figures.

LM4041 LM4041-N
Is there any differens between these characteristic?
Q3. In above explanation, in my understanding, when Vz is set below 2.5V, reference voltage change is increase larger than Vz is above 2.5V.
Is it correct that reference voltage change increase is max -3V as wrote in Electrical Characteristic in datasheet in Vz is below 2.5V condition?
Or in this condiition, reference voltage change is over -3V?
Please your opinion about above.
Best regards,
teritama