Part Number: BQ25619E
Tool/software:
Hello,
I'm testing charging a battery at cool temperature (5°C) and measuring current going to the battery.
The programmed top off timer is 30min.
I expected that at cool temperature the safety timer would be slowed down by 2 so the top off timer would also be slowed down (1 hour).
But charging still stops after 30 minutes.
Here is the i2C register I'm reading just before the charge is stopped:
| REG00 | 0x05 |
| REG01 | 0x1A |
| REG02 | 0x8A |
| REG03 | 0x00 |
| REG04 | 0x9D |
| REG05 | 0x8F |
| REG06 | 0x66 |
| REG07 | 0x55 |
| REG08 | 0x3C |
| REG09 | 0x03 |
| REG0A | 0x88 |
| REG0B | 0x44 |
| REG0C | 0xA5 |
Do you know why top off timer is not becoming 1hour at cool temperature?
Thanks