Other Parts Discussed in Thread: CSD18514Q5A, CSD17578Q3A
Tool/software:
Hi,
Could you please let us know the recommended parts # of FETs on TPS55288 under the following conditions?
- Input Voltage : Min 6V - Max 25.2V
- Output Voltage : 5V/15V/20V
- Output Current : MAX 3A
According to webench, when input voltage is min 8V, webench selects M1:CSD17578Q3A and M2:CSD18514Q5A. However, if min input voltage is 6V, webench does not select actual FET parts #. That is why I am asking.
Thanks and best regards,
M.HATTORI.