Tool/software:
Hello,
In the datasheet, the TYP value for load regulation and line regulation is 1%, but can you tell me the MIN and MAX values?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
In the datasheet, the TYP value for load regulation and line regulation is 1%, but can you tell me the MIN and MAX values?
Thanks!
Hi,
We don't have MIN and MAX values for line and load regulation on the TPS7A16-Q1.
Typical values are measured with bench tests to help provide an estimate of what the value usually is. Min and Max values are guaranteed for the part we ship over the entire test conditions. In this case, we aren't making guarantees about load and line regulation so we cannot provide them.
Best
Gregory Thompson