Tool/software:
Hello,
I want to use LM76202-Q1 for turning ON-OFF the resistive heating element at 10 Hz frequency or periodically at 100ms time. Is there any limitation of e-fuse which I am missing here?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I want to use LM76202-Q1 for turning ON-OFF the resistive heating element at 10 Hz frequency or periodically at 100ms time. Is there any limitation of e-fuse which I am missing here?
Hello Abhishek,
Welcome to E2E.
You will be using SHDN pin to toggle the eFuse at 10Hz I believe.
Are there big capacitors at output? This will cause the eFuse to heat up because of inrush along with resistive load.
If there is very less valued cap, I don't see any limitation for this configuration.
Thanks
Amrit