Other Parts Discussed in Thread: BQ25792
Tool/software:
Hi,
I use the TPS25750 with the BQ25792 in a battery operated device.
The device is strapped for "always enable sink" in dead battery mode.
When the battery is discharging, at a certain moment the main processor stops operating and for some reason the TPS25750 enters BATCH mode ( perhaps by spike on VIN ? ).
Because there is still about 3V on the VIN_3V3 pin, the TPS25750 does not enter dead battery mode.
When I connect a USB power supply, the TPS25750 does not switch the USB power towards the BQ25792, so the battery cannot recharge and the system is therefor in a deadlock.
Is there a way I can resolve that? One nice solution would be to instruct the main processor to put the TPS25750 in dead battery mode when battery becomes dangerously low, but there is no system task for this.
Is there another solution for this problem? Could it be solved by configuring the TPS25750 in "sink only" mode for instance? Now iyt is configured for sink and source.