This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28750: Modifying UCC28750EVM-071 design to take 1200VDC input

Part Number: UCC28750
Other Parts Discussed in Thread: UCC28704, UCC28742, UCC28722

Tool/software:

Hi,

I would like to use the UCC28750EVM-071 design as a starting point for a high input voltage, isolated, DC-DC converter. Input voltage range = 200Vdc - 1200Vdc, output voltage = 24V, max output current = 1.87A. Aside from the obvious component voltage rating modifications what other modifications would need to be made to the UCC28750EVM-071 design to meet this higher input voltage requirement?

  • Also, if there is a component that is better suited for this application, I am all ears.

  • Hello,

     

    6 to 1 is quite a large variation in input voltage.  You might be better designing with a DCM flyback converter that uses variable frequency.  You can do this with a primary side regulated UCC28704 or a UCC28742.

     

    The following link will bring you to an application note that describes how to design a flyback converter for a wide input range using the UCC28722 controller.  However, this same technique applies to the UCC28742 and UCC28704.

    https://www.ti.com/lit/pdf/slua781

     

    If you need further help with either of these devices please repost in the e2e with the part number in the thread title so the appropriate applications engineer can help you with your design.

     

    Regards,