Part Number: UCC28070A
Tool/software:
Dear Team,
I tried making a design using Webench for the below specification considering UCC28070A, link is given below.
(webench.ti.com/.../SDP.cgi
Input voltage - 53Vac (75Vdc) to 70Vac (100Vdc)
Input current - 11A
Output voltage - 350Vdc
Output current - 2.3A
Output power - 800W
Boost efficiency - 95%
But I could not feed input voltage below 64Vac (90Vdc). So, I would like to know if UCC28070A can work for mentioned input voltage range or not.
If controller can work, shall I use SLUC114 sheet and proceed.
Warm regards,
Sakthivishnu