The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: Application issues

Part Number: BQ25703A

Tool/software:

Hi

When using BQ25703A to charge the battery in buck mode, with 20V input and 8V output, there is no abnormality in the waveform of the G pole of the two MOS transistors; If it is boost mode, 5V input, 8V output, and the G poles of two MOS transistors overlap, how to solve this situation because there is a platform voltage on the upper transistor;