This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ41Z50: BQ41Z50 Unused Pin Confiuration

Part Number: BQ41Z50

Tool/software:

Hi Teams,

In the BQ41Z50 datasheet, some unused pins are recommended to be left floating, while others can be connected to VSS through a 20kΩ resistor or left floating.

I have a few questions I'd like to clarify.

  1. Why is there a difference in treatment between unused pins?

  2. For pins that allow a 20kΩ pull-down, can multiple pins share one 20kΩ resistor?

  3. Between floating and using a 20kΩ pull-down, which option is generally preferred?

Thanks.

Best regards,

  • Hello Tom,

    The person that this question has been assigned too is out of office and please allow for some time for him to review this question.

    Thank you,
    Alan

  • Hi,

    Why is there a difference in treatment between unused pins?

    These are requirements from he designs team based on the requirements for the internal circuitry or due to pin functionality. 

    For pins that allow a 20kΩ pull-down, can multiple pins share one 20kΩ resistor?

    I can check with the design team on this.

    Between floating and using a 20kΩ pull-down, which option is generally preferred?

    Please follow the data sheet.

    Regards,

    Diego

  • Hello Tom, 

    From the designer engineer I was able to get this information back from him

    For pins that allow a 20kΩ pull-down, can multiple pins share one 20kΩ resistor?

    "Yes, unused pins make share a single 20k Ohm pull down resistor"

    Why is there a difference in treatment between unused pins?

    "Some unused pins may increase leakage if shorted to ground, please follow the datasheet recommendations for each pin"

    Thank you,
    Alan