This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54338: RT/SYNC Pin Voltage Limits with RC Circuit

Part Number: TPS54338

Tool/software:

Dear Team,

My customer considers to use the TPS54338 with both RT mode and SYNC mode. Datasheet, page 16 to 17, "6.3.5 Switching Frequency Selection / Synchronization" describes the RC circuit "Figure 6-3. SYNC Mode Configuration" which can be used to interface the RT/SYNC pin.

This is AC-coupling circuit. 
Q1: When the SYNC signal amplitude is 0V to 3.3V, what is the amplitude of the RT/SYNC pin input voltage?

Q2: Does the ESD diode of GND-->RT/SYNC conduct every SYNC signal period and clamp the RT/SYNC pin negative voltage to the -Vf voltage?
       Is this behavior a problem for the TPS54338?

Best Regards,

Koshi Ninomiya