Tool/software:
Dear Team,
My customer considers to use the TPS54338 with both RT mode and SYNC mode. Datasheet, page 16 to 17, "6.3.5 Switching Frequency Selection / Synchronization" describes the RC circuit "Figure 6-3. SYNC Mode Configuration" which can be used to interface the RT/SYNC pin.
This is AC-coupling circuit.
Q1: When the SYNC signal amplitude is 0V to 3.3V, what is the amplitude of the RT/SYNC pin input voltage?
Q2: Does the ESD diode of GND-->RT/SYNC conduct every SYNC signal period and clamp the RT/SYNC pin negative voltage to the -Vf voltage?
Is this behavior a problem for the TPS54338?
Best Regards,
Koshi Ninomiya