Other Parts Discussed in Thread: BQ79616
Tool/software:
bq79600 is responding and i am able to read data.
Now I have connected bq79600(COMH_p) to bq79616(COML_P) similarly N. After bq79600 wake ping. I am sending following
81 00 03 09 01 2F 8E
to wake up stack devices. Is this ok or should I send DIR_SEL=1 before this? attaching my schematic..Please check if the isolation transformer (HMU1228NL) is ok?
update:
I have also tried by sending data in the following sequence
Hardware: Removed, transformed,r and connected a 2.2nf i.e used capacitive isolation
Some observed info: bq79616-->COMP,COMN : 2.5V,2.5V bq79600-->COMP,COMN : 2.195V,2.195V
1. Wakeup ping on bq7900
2. DIRE SEL=1: 81 0 3 9 80 EF EE ( As I am using COMHP,COMHN and left COMLN,COMLP unused)
3. Send a wakeup to the stack 81 0 3 9 20 EF 96
Kindly please check where am I gng wrong
Thanks&Regards
Mounish