This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87725-Q1: RSTOUT open-drain configuration and voltage tolerances

Part Number: LP87725-Q1

Tool/software:

I'm working on a design using LP87725-Q1 and would like to use the RSTOUT pin pulled up to 1.8V instead of 3.3V. The RSTOUT pin says it can be open-drain if the internal PU resistor is disabled, which should allow me to do this. What is the default state of that pin with regards to being open-drain vs push pull? And if it's not OD by default, what do I need to do to make that happen? Thank you!

OPN: LP87725110RAGRQ1