Other Parts Discussed in Thread: TPS62825A,
Tool/software:
Hello,
I am measuring efficiency for a 1.5V design using the TPS62825AEVM-126 and I am calculating an efficiency of about 46% at a load of 30mA. According to the TPS62825A datasheet, the efficiency should be a little more than 90% (using figure 8-7, Vin = 3.3V Vout = 1.2V). Increasing the load current improves efficiency but it still does not align with figure 8-7.
Below is what I measured.
Vin = 3.3V
Iin= 0.03A
Vout = 1.524
Iout = 0.03A
Below are the changes I've made to the evaluation board.
C6 = 10uF
C1 = 0.1uF
C5 = 10uF
R1 = 15.4k
R2 = 10K
C3 = 1200pF