This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616-Q1: Maximum chain count with BQ79600-Q1

Part Number: BQ79616-Q1
Other Parts Discussed in Thread: BQ79616, BQ79600-Q1

Tool/software:

How many devices can be chained when using BQ-79600-Q1?
I understand that since the device adress of each of the BQ79616-Q1 is of 8 bits, the device would support upto 255 devices. But in some forum posts its mentioned that:
"Each of our BQ79616 can manage up to 16 cells (80-V max). With our EVMs, you can have up to 35 BQ79616EVM modules stacked, for packs up to 560 series cells."

  • What is the reason for this limit, Is this only with TI's EVM Boards?
  • What considerations are to be made when designing boards for larger chains?
  • Hello, 

    The device address of each BQ79616-Q1 device is 6 bits, therefore supports up to 64 devices. The previous forum post discusses only the EVM stack size.

    Future Considerations:
    For both the BQ79616-Q1 and BQ79616EVM, the device limit of 64 and 35, respectively, would be decreased by 1 if using a bridge device such as the BQ79600-Q1, as it would use the device address 0x00.
    It's also recommended to protect against cable breaks between devices, especially with longer chains, by using a redundant ring architecture. More information on this can be found at the BQ79616-Q1 datasheet.