Tool/software:
Hi all,
Q1: Does this device do I2C clock stretching?
Datasheet section "8.5.1.3 Byte Format" mentions clock stretching in a general way, but it is unclear whether the device actually makes use of it.
Section "8.5.1. Serial Interface" says:
"Due to the ultra low IQ when the device operates in low power mode, it is necessary ensure a minimum of 90μs between a START command and any subsequent START command on the I2C bus."
Q2: What is "low power mode"? I can only find "Shutdown Mode" and "Ship Mode".
Q3: Does the 90µs limitation only apply in "low power mode" (whatever it is)?
Q4: Does it also apply when the device is not addressed at all, i.e. when communicating with other devices on the same bus?
This would be quite a serious limitation.
Kind Regards,
Wolfgang