This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD17318Q2: Chipped corner

Part Number: CSD17318Q2

Tool/software:

Hi,

I would like to inquire what the top of body material to substrate distance is?

Reason: I have a small chip corner on the component that it's still within IPC spec. I would like to know if small chips are reason for replacing the part.

Thank you!

 

  • Francisco,

    I am double checking with manufacturing but I am pretty sure this chip would not have passed our final inspection criteria and so should never have been shipped to you.

    Was this device like this prior to being paced on the board? Or did the device receive some mechanical impact during assembly?

    The corner damage looks like it could have been some sort of impact force, this is the corner where the gate bond wire is located.

    Given the likely severity of the force it is not possible to predict the reliability of the device. These types of impact may produce micro cracks in the silicon/wire bond issues which over time although working fine now may actually fail when the devices is subjected to repeated heating and cooling. It is not possible to predict this, only in application usage would see if this true or not.

    The thickness of the leadframe or substrate is in the datasheet, this is 0.2mm, the chip out is likely very close to the gate bond wire which loops from an internal pad to the silicon die to form the gate connection.

    I am trying to find out how high this loop is however, I would recommend the safest course of action is to replace the device in this case.

    Many thanks for using our device

    Best Regards

    Chris Bull

  • Chris,

    Appreciate the quick response. I believe this happened at our site, due to mishandling. I already relayed the message to our production team to replace the part. 

    Thank you !