Other Parts Discussed in Thread: LM5145, , LM5149
Tool/software:
Hi,
I have been digging around for some details about exactly how TIs family of synchronous buck controllers actually deal with the problem of start up when the output voltage is pre-biased and has a voltage either none zero but below set-point or even where the output is above the desired set-point and is gradually collapsing to below the switcher set-point.
I have found some brief comments regarding the LM5145 behavior.. https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/952519/lm5146-q1-how-does-pre-biased-startup-work
This discusses the idea the the controller monitors the FB voltage and when it is above the ref (either SS or Vref) it recognizes this 'special' condition and switches the on the low side FET until the zero cross detector is triggered. If this is true, at what threshold is the zero cross detection set -5mV, 0mv or 200mV. Normally during SS DEM is forced on and therefore this threshold would be 0mV or very close to 0mV.
The TI expert also describes this as a 'kind of' reverse boost converter action, and this is indeed clear, he then alludes to the problems that could arise from doing this. that being, when the low side FET switches off, it will potentially force current from output to input through the body diode of the high side FET, and maybe even damage the input vin / bias. I assume this is particularly concerning if the input stage is protected with an in line diode, as recommended in the datasheets. I have not attempted any formal analysis of this condition. But I assume as a TI engineer is discussing it. It must be a valid and concerning operation state.
Therefore, is this description accurate? Is this actually how the controller ensures that the bootstrap capacitor is charged? How many times does this switching occur, does it constantly do this until the ref voltage (SS or vref) has risen above the FB voltage?
Or is this entire description describing something that this controller does do, or is the author describing something that has been avoided in the LM5148 by using some alternative approach. It is not clear and to be honest, I still do not have a detailed step-by step understanding of exactly what the controller does to manage these conditions and what I should be concerned about in terms of damage to the IC under all possible scenarios?
Thanks, looking forward to a response.