Part Number: BQ25895
Other Parts Discussed in Thread: TPS566238,
Tool/software:
Q1. Can I get 3.3V from the VSYS pin to power my board? If not, can I use TPS566238 (at VSYS) to get 3.3V, 2A? Any other better suggestions to replace TPS566238.
Q2. Is it safe to copy the layout design of BQ25895EVM completely?
Q3. I have two adapters, A1 can provide 5V/3A, 9V/3A, 12V/3A, 15V/3A. But, A2 can provide 15V/3A only. Considering the recommended limit of 14V on VBUS, if I put a 130-ohm ILIM resistor for a 3A input limit then what voltages will I get if I use A1 and A2?