This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600: LLC half bridge resonant converter

Part Number: UCC25600
Other Parts Discussed in Thread: UCC25640, UCC28180

Tool/software:

Hello,

We are working on LLC half/full bridge resonant converter for one of application,

Where,

Output Voltage is 21KV/ 200W

Input Voltage is 230VAC.

We are considering UCC25600 or UCC25640.

Can you help us is we are selecting right controller and share if any supporting reference design 

Thank you,

Supriya,

  • Hello,

     

    Your inquiry has been received and will be reviewed and addressed in the order it was received.

     

    Regards,

      

  • Hello,

     

    I searched the reference design library and TI has not done any reference designs for a 230 V AC to 21 kV output.  We do have a lot of experience in off line power but typically the output voltages we deal with are less than 1000 V DC.  So, I don’t believe we have specific power supply controllers made for this application.

     

    You might be able to achieve this with a UCC25600 at 200 W in an LLC using Fets on the primary and high voltage high speed rectifiers on the secondary.  LLC converters are generally limited to a 2 to 1 input variation.   So, to avoid these issues you might want use a PFC front end.  A UCC28180 could work here and I would set the output voltage to 390 V.

     

    Regards,